Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29
About this task
Note: You cannot create a new archive database if another archive database is
already open. You are prompted to close any open archive database before creating a new
archive database.
Procedure
From the Item menu, select New Archive.
The New Archive wizard screen appears.
Enter a name for the new archive. Note the following restrictions:
Archive names are not case sensitive. All archive files are created in the same
directory.
Archive names cannot be longer than 120 characters.
The first character can only be an alphabetical character from a to z.
No special characters can be in the name. For example, ! @ # $ % . and & are
not allowed.