Copying an Archive Database - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

The Archive copy must have a unique name. By default, the new archive has the same name as the one you are copying with a number appended to the name.

To copy an archive database:

Procedure

  1. With an archive database open, select Create Archive Copy from the Item menu. The Copy Archive wizard appears.
  2. Select the archive to copy from the list.
  3. Type a name for the new Archive database copy in the right pane of the wizard.
  4. Click Copy.
  5. Click Yes when prompted to close the current database. The new Archive copy opens.