Menu Selection:
Creates a copy of the existing and currently open archive database in the SCT.
The copy is intended as a second backup in case the original backup file is deleted. Do not rename the backup file because the file does not restore properly using a different name (it is case sensitive). If you want to rename a backup file, create a copy of the archive and give it the new name before you create a backup. You cannot rename the backup after it is created.