Viewing Trend Studies - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

Note: To create Trend Studies, see Creating Trend Studies (Overview).

Procedure

  1. From the navigation tree, drag the Trend Study you want to view to the Panel Layout.
  2. Select the Definition View button to edit the Trend Study. Select the Chart View or Table View buttons to view the trend data.

Results

Notes:
  • The UI limits the number of data samples you can retrieve. Therefore, you may not see the full range specified. The most recent data samples are always retrieved first.
  • If the chart appears to flicker, you have too many trend samples in the Trend Study. Reduce the number of displayed trends or change the trending date/time range to display fewer samples and improve performance. See Deleting Trends from the Trend Study.