Adding New Trend Items to the Trend Study - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0
SCT: System Configuration Tool Help
- Product
- Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
- Document number
- LIT-12011964
- Version
- 16.0
- Revision date
- 2023-09-29
Procedure
-
View the Trend Study.
-
If necessary, click the Definition View button.
-
Click the Edit button in the upper left of the Trend
Study tab.
-
Click the Add icon in the Trend Items
table. The Select Item dialog box appears.
-
Select the trend(s) that you wish to add from the Select Item
dialog box.
Notes:
- Multiple selection adds multiple items.
- All non-trend items
appear dimmed. If everything appears dimmed in the Select Item dialog box, check to
see if you have at least one object with a Trend Extension and/or that Engine
devices from other sites are storing samples in the Metasys server
(if applicable).
-
Click the OK button in the Select Item
dialog box.
-
Click the Save button in the Definition
View to save the changes.