The Trend Items table appears at the bottom of the Definition view. The Trend Items table displays the list of the Trend Study’s trend items.
|
Button |
Name |
Description |
|---|---|---|
|
|
Historical Trend Icon |
Indicates the trend was selected from the Metasys server Historical Database folder. |
|
|
Add |
Opens the Select Item dialog box and allows you to add trend items to the Trend Study. This button only enables when the view is in edit mode. Note: All items and navigation trees appear in the Select Item window; however, you can only select trends. All other items appear dimmed.
|
|
|
Remove |
Allows you to remove a trend item from the Trend Study. This button only enables when the view is in edit mode. |
|
Name |
Displays the name of the trend item. |
|
|
Reference |
Displays the trend item’s reference information. |
|
|
Aggregate Function |
Allows you to select the aggregate function to use on the trend sample data (NONE, Average, Minimum, Maximum, Standard Deviation, Range, Sum, and Variance). You can sample the same point for different aggregate functions and display them on a single chart. Aggregate functions group multiple values together to construct a single value that has significant meaning or measurement. Descriptions of available aggregate functions are as follows:
The aggregate functions of the trend study apply to information in the Historical Data at the Metasys server server and do not apply to data in the NAE buffer. |
|
|
Aggregate Interval |
Specifies the time, in minutes, over which the aggregate function should be applied (for example, 60 for an hourly calculation, or 1,440 for a daily calculation). |
|
|
Plotting Style |
Allows you to select the plotting method for the trend item.
|