Trend Studies - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Accessible through the navigation tree, Trend Studies display trend sample data from trends in Engine trend buffers and/or Metasys server repositories. A Metasys server on the site is not required to retrieve trend data from the Engine.

When you create a Trend Study, you use the Trend Study wizard to choose the sources for the trends and the display properties.

An Audit Trail message is created whenever you create, delete, or edit a Trend Study. Trend Studies, graphics, and folders are the only items you can create under a Metasys server on the navigation tree.

The main advantages to using Trend Studies are that you can:

  • view multiple trends at once (from both Engine and Metasys server )

  • view Metasys server historical trend data

  • configure the Study Range with flexible parameters

Note: You do not need a Metasys server on the site to forward trend samples to a Metasys server . You can forward trend samples to a Metasys server on a different Metasys site. See the Metasys Server for Metasys server information.