Archive - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

A copy of the database, called the archive, is kept in each Engine’s flash memory. This happens automatically once a day or on operator command. Following restoration of power loss to an Engine, the archive is copied into main memory to restore normal operation.