Supervisory Device - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Menu Selection: Insert > Supervisory Device

Inserts a supervisory device into the archive database with SCT.

Metasys System: NAE35, NIE39, NAE45, NAE451L, NIE49, NAE55, NIE59, NAE85, NIE89, NCE25, NIE29, NIE55, NIE85, SNE10/SNE11/SNE22, and SNC16/SNC25. You can insert a device at a previous Metasys system release with SCT, beginning with Release 5.2 and later. The SNE and SNC devices are only available to SMP at Release 10.1 or later, and SCT Release 13.2 and later.

FX System: SNC16 and SNC25.

Note: The Metasys NAE451L and SNE110Lx network engines are available only to select regions of Australia, China, Hong Kong, India, Indonesia, Japan, Korea, Malaysia, New Zealand, Philippines, Singapore, Taiwan, Thailand, Vietnam, and select branches.

On the Configure screen of this wizard, click any tabs that may appear for further device configuration.