The Summary Definition Editor’s Summary Definition tab allows you to define the table that appears in the Tailored Summary view.
|
Button/Field |
Description |
|---|---|
|
Label |
Defines the label to display in the first column (that is, the row header column) in a Tailored Summary. The label is limited to a maximum of 50 characters. This field also can be left blank. |
|
Add/Plus |
Allows you to add a column at the end of the column configuration table.
Note: You can define up to a maximum of seven columns. This button is disabled
if seven columns already exist.
|
|
Remove/Minus |
Allows you to remove the currently selected column from the column configuration
table.
Note: To select a column, click the column heading. You must define a
minimum of at least one column.
|
|
Column Configuration Table |
Lets you configure the columns that appear in the Tailored Summary:
Notes:
|
|
Browse (Child Item) |
Opens the Select Item dialog box where you can specify the item name.
Note: This
dialog box provides an easy way to fill in the item name of a child item. It
does not mean that the selected item displays in that column.
|
|
Browse (Attribute) |
Opens the Select Column Attribute dialog box where you can select the attribute to display in the column of the table. This process is necessary only when selecting an attribute other than the default attribute. This dialog box has two list boxes to aid in selection:
Note: To display the default attribute of the row item, leave the Attribute box set
to Default (Attribute Filter: Common Attributes and Attribute: Default).
For an example of the attributes available for display in the Tailored Summary feature, see the Tailored Summary Attributes section. |