Focus Tab - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Summary Definition Editor’s Focus tab allows you to define the Key Data that appears outside the main table in the Tailored Summary view, as well as other common Metasys object attributes. To define Key Data, click the Browse button of the Key Data attribute on the Focus tab. This action opens the Modify List dialog box.

The Object Name attribute on the Focus tab provides the name shown in the Summary Definition folder in the All Items tree.

Figure 1. Modify List Dialog Box

Table 1. Modify List Dialog Box

Button/Field

Description

Key Data List (Listof[x])

Displays the added Key Data items. You can use the Select Item dialog box to pick the Key Data item, or type in the text box. You also can use wildcards (asterisks * only), where the system searches for the matching item in the user view folder. You can define up to four Key Data items.
Note: The default attribute of the Key Data item appears in the Key Data table of the Tailored Summary view.

Browse

Opens the Select Item dialog box for selection of the Key Data item.

Add

Adds an undefined item to the Key Data list.

Remove

Removes the currently selected item from the Key Data list.

Move Up

Moves the currently selected item up one place in the Key Data list.

Move Down

Moves the currently selected item down one place in the Key Data list.

Cancel

Closes the dialog box without accepting the changes.

OK

Accepts the changes and closes the dialog box.