Create New Summary Definition Wizard - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Use the Create New Summary Definition Wizard to create a Summary Definition object from scratch. Access this wizard using the Summary Definition option on the Insert menu.

Table 1. Create New Summary Definition Wizard

Screen

Description

Identifier

Allows you to enter a name for the Summary Definition object.

Configure

Allows you to define the data of the Summary Definition and Configuration tabs.
Note: The Configuration tab in this wizard contains the same data as the Focus tab of the Summary Definition Editor.
See the Editing an Existing Summary Definition and Defining Key Data sections for details on how to edit these items.

Summary

Displays the summary data of the Summary Definition object.