Site - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Menu Selection: Insert > Site

Inserts a site into the archive database in the SCT.

Tip: The Create Device? dialog box appears after inserting a site that asks if you want to create a device in the site. To invoke the Insert Device wizard, select Supervisory Device, then click OK. To invoke the Insert Metasys Server wizard, select Metasys Server, then click OK. If you do not want to add a device at this time, select None, then click OK.