This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Attributes section. For information on the Tailored Summary Viewer feature, see Tailored Summary Viewer.
Click the attribute name in the table for a description of the attribute.
|
Attribute Name |
Data Type |
Notes |
Initial Value |
Values/Options/Range |
|---|---|---|---|---|
|
Name |
Text |
CW |
Maximum Length of 400 characters |
|
|
Description |
Text |
CN |
Maximum Length of 40 characters prior to Release 8.0 and 64 characters at Release 8.0 and later. |
|
|
Authorization Category |
One type from a set |
C |
General |
HVAC, Fire, Security, Services, Administrative, General Lighting, Refrigeration, Critical Environment, Air Quality, Power, Energy, System Custom 1-150 |
|
Attribute Name |
Data Type |
Notes |
Initial Value |
Values/Options/Range |
|---|---|---|---|---|
|
Column Heading |
List of Structures |
C |
Column Heading, Child Item, Attribute |
|
|
Row Headings Column Text |
Text |
CN |
Label Maximum Length of 50 characters |
SCT Summary Definition Attribute Details
- Column Heading - Defines the name of the column header.
- Child Item - Indicates item for which the column data is retrieved based on its name attribute, which must match a user-specified pattern (such as ZN-* or ZN-T, or Zone-T). To display an attribute of the row item, leave this field blank. Otherwise, specify the name of the child item to display.
- Attribute - Defines the attribute information for the column. The attributes are grouped into categories for easy selection. Select a category in the Attribute Filter section of the Select Column Attribute dialog, and then select the desired attribute from the list.