Program Change - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English
  • Ready - Specifies that the LCT control system is ready for a change request (normal state).

  • Load - Enables the LCT control system.

  • Run - Enables the LCT control system.

  • Halt - Disables the LCT control system.

  • Restart - Disables, then Enables, the LCT control system.

  • Unload - Disables the LCT control system.