Program Object - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Program object (previously the Control System object) stores information needed for the user-defined control strategies created (graphically) with the Logic Connector Tool (LCT). The Control System object application now includes BACnet command object functionality and appears as the Program object in the Metasys software. The Program object attributes allow manipulation of the LCT application.

For general information on Metasys system objects, see Common Object Attributes.