Saving a Control System - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

To save a control system, click Save on the Toolbar. The LCT scans for logic errors.

Notes:

  • The logic check done with the Save command is not the same as the Logic Checker run from the toolbar.
  • If inputs are missing, an error message appears asking if you want to continue with the save. Click No to return to the logic. Click Yes to save anyway. We do not recommend saving with errors.