Editing TMR (Timer) Blocks - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

About this task

To edit TMR (Timer) blocks in Edit mode:

Procedure

  1. Double-click a Timer block. The TMR dialog box appears.
  2. Edit the timing functions of the block.
    Table 1. TMR (Timer) Block Configuration

    Field

    Description

    Duration

    Specifies the length of the timer function in seconds. The range is 5–86,400 seconds.

    Setup

    Determines the type of timer you use:

    • Pulse
    • On Delay
    • Off Delay
    • Minimum On
    • Minimum Off

    OK

    Accepts changes.

    Cancel

    Cancels changes.