Editing Statistical Blocks - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

To edit Statistical blocks in Edit mode:

Procedure

  1. Double-click a Statistical block. The configuration dialog box appears.
  2. Edit the fields and configure the type of statistical block and number of inputs.
    Table 1. Statistical Block Configuration

    Field

    Description

    Type

    Allows you to switch between the statistical types.

    Input

    You cannot reduce the input count lower than the number of current connections.

    OK

    Accepts changes.

    Cancel

    Cancels changes.