Editing Control Blocks - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

To edit Control blocks in Edit mode:

Procedure

  1. Double-click a Control block. The configuration dialog box appears.
    Note: See Editing SEQ (Sequencer) Blocks for Sequencer configuration information.
  2. Edit the fields to configure the type of comparison.
    Table 1. Control Block Configuration

    Field

    Description

    Type

    The Type of comparison performed by the block. This field defaults to what was dragged over, but may be changed.

    OK

    Accepts changes.

    Cancel

    Cancels changes.