Editing Constant Blocks - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

To edit Constant Category blocks in Edit mode:

Procedure

  1. Double-click a Constant block. One of two dialog boxes appears depending on the type of constant you select.
    Note: There are no configurable parameters for the Rel. (Release) constant. When you double-click, nothing happens.
  2. Edit fields and configure the constant value (Editing Constant Enum, Editing Constant Float).