Editing Span Blocks - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

About this task

To edit Span blocks in Edit mode:

Procedure

  1. Double-click a Span block. The Span dialog box appears.
  2. Edit the fields to enable or disable clamping.
    Table 1. Span Block Configuration

    Field

    Description

    Clamp High

    Selects whether (True) or not (False) to clamp the Output at the Output High (OH). For more information on clamping, see Span.

    Clamp Low

    Selects whether (True) or not (False) to clamp the Output at the Output Low (OL). For more information on clamping, see Span.

    OK

    Accepts changes.

    Cancel

    Cancels changes.