Procedure
- Double-click a Bool block. The configuration dialog box appears.
-
Edit the fields and configure the number of inputs based on the selected type of Boolean logic.
Table 1. Bool Block Configuration Field
Description
Input
The number of inputs depends on the type of Bool block you use. You cannot reduce the input count lower than the number of current connections.
OK
Accepts changes.
Cancel
Cancels changes.