Editing Attribute Outputs - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29
Table 1. Attribute Output

Field

Description

Name

Name of the output

Units

The units for the output

Display Precision

Tells the Metasys software what precision to use when formatting data.

This field only appears for floating outputs.
Note: Display Precision is used in the Focus view of data, not the graphical view.

Enum Category

Set category determined by the user interface (either Two State or Multi State).

This field only appears for Enum outputs.

Enum Set

Set determined by the category selected in Enum Category.

This field only appears for Enum outputs.

OK

Accepts changes.

Cancel

Cancels changes.