Re-Routing a Connection - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Procedure

  1. Make sure the LCT is running in Edit Mode.
  2. Place the cursor over an existing end connection point until the cursor changes into a cursor with lines protruding from the tip.
    Note: You may only move the destination point. To completely change the connection, see Deleting Connections.
  3. Click the connection point. The tool removes the connection.
  4. Click a new connection point. The tool creates the newly routed connection.