Hiding Output Connections - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Procedure

  1. Make sure the LCT is running in Edit Mode.
  2. Place the cursor over the output connection point and right-click and a menu appears.
  3. Select Hide from the menu. The tool removes all connections from the output and replaces the lines with numbered symbolic representations of the connections.
  4. To see the connections again, right-click the starting connection point and select Unhide.
    Note:

    Double-click the hidden connection to label it. If multiple connections are from the same hidden input, it is shown as Label: number where number is the number of connections.

    Do not start labels with a number and then follow it with any of these characters: $ . - ,