Connecting Blocks - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Procedure

  1. Make sure the Logic Connector Tool is running in Edit Mode.
  2. Place the cursor over the starting connection point until it changes shape from an arrow to a magic wand and click the point.
  3. Click the ending connection point.

    Notes:

    • If the connection is valid, the cursor is a magic wand. If the connection is not valid, a circle with an X through it appears, and the tool does not connect the points.
    • After you successfully connect two points, the line between them turns blue until you click somewhere else in the workspace.
    • You do not need to click the exact connection point. If you click in the block, the tool automatically creates a connection to/from the nearest block’s connection point. To cancel the connection after clicking the first block, click anywhere in the workspace.
  4. The Priority Connection dialog box appears. Choose a priority from 1–16 (1 is the highest priority).
    Note: To change the priority at a later time, you must delete the connection and reinsert it.