Copy and Paste - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

About this task

Note: You can copy and paste existing objects into the workspace from the workspace only.

To add items to a control system using the copy and paste method:

Procedure

  1. Right-click an existing object and select Copy.
  2. Right-click in the workspace and Paste the object.
    Note: The copy and paste method supports copying and pasting of multiple blocks. To copy and paste more than one block, hold down the Shift key while selecting blocks with the cursor or use the select tool to lasso the blocks.