The following table shows describes the LCT toolbar:
Note: If you click outside of the display panel containing the logic system, when you
use a zoom tool in View mode, the zoom level automatically changes back to the
default.
|
Icon (Standard Windows Icons not Shown) |
Command |
Visible In |
Action |
|
|---|---|---|---|---|
|
Edit Mode |
View Mode |
|||
|
|
Edit Mode | X | Changes the control system to Edit mode. | |
|
|
Refresh | X | Refreshes the values for control system components. | |
|
|
Save | X | Saves the logic system and changes it to View mode. If there are unconnected points, the logic system warns to fix them prior to a save. | |
|
|
Cancel | X | Cancels current changes and returns to View mode. | |
|
|
X | X | Print dialog appears | |
|
|
Print Preview | X | X | Print Preview dialog appears |
|
|
Cut | X | Cuts an item of the control system. | |
|
|
Copy | X | Copies an item in the control system. | |
|
|
Paste | X | Pastes a cut or copied item into the logic system. | |
|
|
Undo | X | Undoes the previous action (except for a save) for up to 4 actions. | |
|
|
Redo | X | Redoes the previous undone action (for up to 4 actions). | |
|
|
No Grid | X | Removes the grid from the diagram. | |
|
|
Lines Grid | X | Displays a line grid behind the diagram. | |
|
|
Points Grid | X | Displays a point grid behind the diagram. | |
|
|
Select | X | X | Turns the cursor into a selection cursor. |
|
|
Text | X | Turns the cursor into a text cursor that allows you to create a text box. | |
|
|
Pan | X | X | Turns the cursor into a hand that allows you to pan over the diagram by dragging. |
|
|
Zoom | X | X | Zooms a selected area. |
|
|
Interactive Zoom | X | X | Zooms in and out on a diagram when you hold the mouse down. |
|
|
Zoom - Fit Window | X | X | Zooms the diagram to fit within the window. |
|
|
Trace Mode | X | Removes all the connection lines in the diagram. Live values remain. | |
|
|
Selective Zoom | X | X | Allows you to select the percentage zoom applied to the diagram. |
|
|
Logic Checker | X | Checks the control system logic and places a balloon with an icon over unconnected points. See the Logic Checker section. | |
|
|
Sequence (Show Sequence Order) | X | Shows the logical sequence order of the connected blocks. A value of -1 indicates that logic does not execute on the block. | |
|
|
Overview | X | X | Shows an overview of the entire control system. |