TMR (Timer) - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

This table describes the components of the TMR blocks:

Table 1. TMR (Timer) Blocks

Output

Description

IN

Input

RS

Reset. Cancels the timer. Reset does not apply to Minimum On or Minimum Off timers. Use a binary object attribute for Reset (1.0=Reset Active, 0.0=Reset Inactive).

The LCT contains five different types of timers. Each type uses a Duration (how long the timer is active) and unique functions to generate an Output. The different types of timers are listed below. Click the name of the timer for a description and figure of timer operation.

For information on setting Duration and the type of Timer, see Editing Timing Blocks.