Minimum On Timer Function - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The following table and figures illustrate the function of the Minimum On timer.

Table 1. Minimum On Timer Function

Feature

Description

Activation

See row below.

Output

Goes active when there is a low to high Input transition when the timer executes (logic executes every 5 seconds). The Output remains active until the time specified in Duration passes AND the Input returns to inactive.

Reset

Has no effect on Minimum On timer.

Example

Keeps a chiller running for a minimum time after startup to stabilize equipment.

Figure 1. Minimum On Timer Example 1

Figure 2. Minimum On Timer Example 2