The following table and figures illustrate the function of the Minimum Off timer.
|
Feature |
Description |
|---|---|
|
Activation |
See row below. |
|
Output |
Goes inactive when there is a high to low Input transition when the timer executes (logic executes every 5 seconds). The Output remains inactive until the time specified in Duration passes AND the Input returns to active. |
|
Reset |
Has no effect on Minimum Off timer. |
|
Example |
Keeps a chiller off from a minimum time after shutdown to equalize refrigerant. |
Figure 1. Minimum Off Timer Example 1

Figure 2. Minimum Off Timer Example 2