Statistical Category - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Statistical blocks perform statistics on input. The number of inputs to a Statistical logic block depends on the number of inputs supported by the type of statistic. The Logic Connector Tool allows you to add multiple connections to the output of the block.

Table 1. Statistical Block Connections

Statistical Type

Inputs

AVG

2–8

MAX

2–8

MIN

2–8

See Editing Blocks in Edit Mode for information on editing Statistical blocks.