Bool Category - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Bool blocks apply Boolean functions to input. The number of inputs to a Bool logic block depends on the number of inputs supported by the type of Boolean function. The Logic Connector Tool allows you to add multiple connections to the output of the block.

Table 1. Bool Blocks

Bool Type

Inputs

AND

2–8

OR

2–8

XOR

2

NOT

1

LTCH

See LTCH (Latch) for details.

See Editing Blocks in Edit Mode for information on editing Bool blocks.