Logic Connector Tool Workspace - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Logic Connector Tool runs inside an active display panel. The workspace for the Program (Control System) Object defaults to a white background. You have the option to add a lined or dotted grid to the workspace using the appropriate buttons on the Toolbar. The workspace displays all building blocks and the connections between them, and serves as the destination for dragged and dropped blocks.