Logic - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Logic contains the following components:

Once a logic process completes, it runs again in approximately 5 seconds. For example, if a logic process starts at 10:00:00 and completes at 10:00:04, it runs again at 10:00:09. It is important that control applications that require particular timing use internal logic to determine time between execution.

If your logic references multiple Engines or multiple Metasys server s, and one device needs to be downloaded, upload all Engines and Metasys server s prior to making changes in SCT. This procedure ensures your logic works consistently.