LCT modes - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The Logic Connector Tool runs in either Edit Mode or View Mode.

You can generate logic and make logic changes in offline mode (SCT) or online mode (SMP). (See Modes.) After generating logic or making any changes to existing logic in offline mode, download the database to the online device to ensure the latest information is used.