Connections - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

Connection lines connect blocks in the logic. The LCT does not do a datatype check; that is, you can connect Boolean and Constant values, and any other combination. But, the tool does not allow inputs to connect to inputs, or outputs to outputs. The tool determines the connection line routing, and the only way to change the routing is to move the blocks or use the hide feature.