This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section.
| Name / View Group
Attribute ID Writable (W) Configurable (C) |
Attribute Description |
|---|---|
|
Input List -- Engineering Values 1062 W C |
Contains the list of attribute references used in the Signal Select calculations. An analog type defined as a binary input is converted to a binary value prior to each computation, and vice versa. |
|
Average Output -- Engineering Values 1063 W C |
Specifies the object attribute whose value is updated using the calculated average of all of the inputs of the Signal Select Object. |
|
High OR -- Engineering Values 1064 W C |
Specifies the object attribute whose value is updated using the highest input of all the inputs in the Signal Select object, for analog point types. For binary point types, the value is updated using a logical OR condition of all inputs of the Signal Select object. |
|
Low AND -- Engineering Values 1065 W C |
Specifies the object attribute whose value is updated using the lowest input of all the inputs in the Signal Select object, for analog point types. For binary point types, the value is updated using a logical AND condition of all inputs of the Signal Select object. |
|
Point Type -- Engineering Values 1173 W C |
Specifies the type of input values monitored by the Signal Select object, the calculations it performs, and the outputs it produces. Point type can be analog or binary. |
|
Failsoft -- Engineering Values 2567 W C |
Routes to all the outputs if Setup is configured as Fail Soft. Fail Soft routes when the object becomes unreliable and when the output transitions from Reliable to Unreliable. |
|
Setup -- Engineering Values 518 C |
Defines whether the Fail Soft or Last Reliable value needs to be the output if the object becomes unreliable. |
|
Execution Priority -- Execution 2197 W C |
Indicates the relative importance of performing the function of the object within the device. |