Pulse Meter Commands - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

The table below lists the commands supported by the Pulse Meter Object.

Table 1. Pulse Meter Object Commands

Command Name

Parameters

Command Description

Enable

None

Enables the calculation of the pulse count and consumption for the Pulse Meter object.

Disable

None

Disables the calculation of the pulse count and consumption for the Pulse Meter object.

Reset

None

Resets the Pulse Meter, including the Consumption attribute.

Start Meter

None

Resumes metering.

Stop Meter

None

Stops metering.