Building an Optimal Start Application - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

About this task

To build an Optimal Start application:

Procedure

  1. Add the N2 Controller object and the analog and binary objects required for the OST application to the database. See the Object Help section for information on objects and the Related documentation table in the Welcome section for information on the SCT. See Creating Items with Wizards for information on creating objects and other items.
  2. Add the Schedule Object , referencing the binary object controlling Zone Occupancy Mode.
  3. Make sure valid occupied and unoccupied times are entered into the Schedule object.
  4. Add the Optimal Start Object referencing the above Schedule object, the Binary objects designated as Zone Occupancy Mode and Zone Warmup or Cooldown Mode, and the analog attributes of objects designated as temperatures and setpoints.

Results

Note: Refer to the Scheduling section in the Metasys SMP Help (LIT-1201793).