Multiple Command Attributes - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Note: In the Notes column, letters indicate the following: In the notes column, letters indicate the following: C - Configurable, D - Default Attribute for Display, N - Value Not Required, R - Affected by Extension’s Reliability, W - Writable.
Table 1. Multiple Command Object Attributes - Focus/Configuration Tab

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Enabled

     

Indicates whether the Multiple Command object is enabled or disabled.

Executing

 

False

False, True

Specifies the current execution status of the object. It is True when the object receives a state command and starts sending commands. When all actions are completed for a given state, this flag is set to False.

Execution Priority

C,W

   

Indicates the relative importance of performing the function of the object within the device.

Last Executed Date

N

   

Indicates the date stamp for the beginning of executing the current state.

Last Executed Time

N

   

Indicates the time stamp for the beginning of executing the current state.

Table 2. Multiple Command Object Attributes - Action Tables Tab

Attribute Name

Notes

Initial Value

Values/Options/Range

Description

Action Table (State0. . . StateN)

C,W

 

Object Reference, Delay, Command ID, Parameters, Priority

Lists actions to take for each supported state. Each action of the table contains a subordinate object reference, a delay, a command and its associated parameters, and a priority. The priority in this table is used only when Commands Priority is set to No Priority. The delay is the number of seconds before the given command is issued. Command delays can be lengthened or shortened to result in commands being sent out after, before, or at the same time as any other command.

The total number of commands identified in the Action Table command set should not exceed 40.

Command Priority

C,W

16

Uses Write Priority (Set 1).

Determines the order by importance for all commands sent. If it is set to Priority None, commands will be sent at each individual priority specified in the Action Table attribute.

Number of States

C

4

1–32

Specifies the number of possible states this object can have.

Relinquish Default

     

Specifies the default value to be used for the Present Value attribute when no commands are currently controlling this object. If this attribute is configured to any value other than None, the object sends commands for the value immediately.

States Text

C

States

 

Indicates the displayed strings for the Present Value.