Multiple Command Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Menu Selection: Insert > Object > Multiple Command

Note:
  • On the Configure screen, click the Action Tables tab for further configuration.
  • Select or enter the desired value for the Relinquish Default. Edit the States Text and Number of States attributes on the Focus tab.
  • Check the All Commands Priority check box if you wish to use the same priority for all commands. Clear the All Commands Priority check box to enable individual priority selection for the commands.
    • For each of the Actions for Condition (State 0 - State N) tables, click the Add button to add items to the table from the Select Item navigation tree.
      • For each of the Actions for Condition (State 0 - State N) tables, click the check box next to an item in the table and click Delete to remove the item from the table.

The Multiple Command object issues a series of commands to multiple objects by means of a single command action. Commanding this object results in the execution of the commands for the given state. This object supports States 1–32.

This object allows a user to start building controls for the day with one command or to prevent selected points from generating COS and alarm messages when a control point is in a specified state (Auto Shutdown).

For example, based on a single input, such as Room Occupied, a defined set of actions can occur: setpoint goes to 72˚, a fan comes on, lights come on, and the door unlocks.

For general information on Metasys system objects, see the Common Object Attributes section.