Global Data Attributes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes unique to the Global Data object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Table 1. Global Data Object Attributes
Name / View Group

Attribute ID Writable (W) Configurable (C)

Attribute Description
Enabled -- Object

673 C W

Indicates whether the Global Data object is enabled or disabled
Set Up -- Engineering Values

518 C

Defines whether the Fail Soft or Last Reliable value needs to be the output if the object becomes unreliable.
Manager -- Engineering Values

1059 C W

Contains an attribute reference. The value associated with this attribute is written to each of the designated subordinate destinations.

Alternate Manager -- Engineering Values

895 C W

Defines an alternate to the Manager. When the Manager becomes unreliable, this attribute becomes the manager attribute.
Subordinates List -- Engineering Values

1061 C W

Contains a list of attribute references. Each subordinate identified in this list of attribute references receives its value from the Manager.

Refresh Timer -- Engineering Values

2325 C W

Indicates the amount of time, in minutes, between updates to the subordinates from the Manager or Alternate Manager. Updates initiated by the refresh timer occur in addition to updates initiated by a COV from the Manager/Alt Manager. For example, if the Refresh Timer attribute’s value is 2, the Global Data object updates the subordinates with information from the Manager/Alt Manager every 2 minutes and with each COV.

If this attribute is set to zero instead, updates are only sent upon receipt of additional COV reports.

Failsoft -- Engineering Values

2567 C W

Routes to all the outputs if Setup is configured as Fail Soft. Fail Soft routes when the object becomes unreliable and when the output transitions from Reliable to Unreliable. This attribute is initialized to a specific value.

Priority For Writing -- Engineering Values

88 C W

Defines the priority at which the referenced attributes are commanded. Seven is the highest priority and 16 is the lowest supported by the Global Data object, with the default of 15.

Note: We do not recommend using priorities 7 or 8 as they may interfere with the operator override function.
Execution Priority -- Execution

2197 C W

Indicates the relative importance of performing the function of the object within the device.