Global Data Object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Menu Selection: Insert > Object > Global Data

The Global Data object provides a means for distributing information about changes in a single attribute value to other attribute reference points. This minimizes hardware costs and system complexity. For example, an NAE might have multiple AHUs on its network, but only one has an outdoor air sensor. The Global Data object can share the value from the single sensor with the other AHUs.

The data types defined for the Global Data object’s input and corresponding outputs should match. Otherwise, each output attempts to convert the value being received to the data type defined for it. The software does not check for data type consistency. Global data sharing is restricted to within one site.

For general information on Metasys system objects, see Common Object Attributes.