Auto Shutdown Attributes - Metasys - LIT-12011964 - Software Application - SCT System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Product
Building Automation Systems > Configuration and Programming Tools > SCT System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-09-29

This object contains attributes common to many Metasys system objects. These additional common object attributes are described in the Common Object Attributes section.

Table 1. Auto Shutdown Attributes
Name / View Group

Attribute ID Writable (W) Configurable (C)

Attribute Description
Enabled -- Object

673 W C

Indicates whether the Auto Shutdown object is enabled (True) or disabled (False).
Control -- Engineering Values

887 C

Determines, in conjunction with the Shutdown State, if an alarm shutdown should occur. This is the current state of the references control point.

Dependents -- Engineering Values

888 W C

Uses each dependent object identified in this list of object references to locate the Alarm object that is to have its alarm reporting controlled by the control point.

Number of Entries = 1–32

Shutdown State -- Engineering Values

889 C W

Determines the definition of the shutdown state. When the control point goes to the state defined as the shutdown state, Auto Shutdown disables alarms from the point.

Startup Delay -- Engineering Values

890 W C

Represents the time in minutes that must elapse before alarm reporting is re-enabled, once the control point changes from the Shutdown State to any other state.

Units = Minutes

Execution Priority -- Execution

2197 W C

Indicates the relative importance of performing the function of the object within the device.