SC Network Port - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The SC Network Port object manages the communication with a BACnet/SC network.

For general information on system objects, see the Object Help section.

For detailed information on the SC Network Port object, see SC Network Port Attributes.

Note: You can see the SC Network Port attributes in the configuration views in SCT, however, the actual configuration of BACnet/SC occurs online using the BACnet/SC configuration as part of Metasys UI (MUI). You can also configure BACnet/SC in JCT to connect to engine only sites that don't have MUI. Refer to Metasys UI Help (LIT-12011953) and Johnson Controls System Configuration Tool (JCT) Help (LIT-12012116).