Mapped Points - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

Existing features of the Metasys system are supported by moving their functionality to the host NIE. These features are: trend, totalization, point history, and scheduling. When possible, existing objects maintain their configuration parameters in the new Metasys system. For example, alarm limits, alarm state, and units. The table below lists points specific to the Metasys system.

Table 1. Mapped Points

Existing Metasys System Object

New Metasys System Mapped Object

Accumulator Object

N1 Pulse Counter Object

Analog Input

Analog Input Object

Analog Output

Analog Output Object

Analog Data

Analog Output Object

Binary Input

Binary Input Object

Binary Output

Binary Output Object

Binary Data

Binary Output Object

Control System

Generic Integration Object (GIO)

Multistate Input

Multistate Input Object

Multistate Output

Multistate Output Object

Multistate Data

Multistate Output Object