LON Integration Attributes - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

This object contains attributes common to many Metasys system objects. These common attributes are described in the Common Object Attributes section. This section includes attributes of the Focus/Configuration tab, the Diagnostics tab (if applicable), and any other tab specific only to this object. See the Object and Feature Tabs section for information on the attributes that appear on the other tabs of this object (for example, the Hardware and Options tab appear on point objects).

Table 1. LON Integration Attributes - Diagnostic Tab

Attribute Name

Data Type

Description

Bind Retry Count

Number

Indicates the number of objects for which the Lon Integration code is still verifying with the field controller that it has the correct type information.

Count

Number

Displays the number of LonWorks network point object defined for the trunk.

Device Offline Polling Cycle Time

Number

Indicates how often all offline devices are polled.

Device Online Polling Cycle Time

Number

Indicates how often all online devices are polled.

Error Log

One value from a set

Shows the error log according to the last standard LonWorks network Query Status message.

LON Integration DLL Date

Date

Displays the current date stamp on the LonIntegration.DLL.

LON Integration DLL Size

Number

Displays the current size of the LonIntegration.DLL.

LON Integration DLL Time

Time

Displays the current time stamp on the LonIntegration.DLL.

Lost Messages

Number

Shows the number messages lost according to the last standard LonWorks network Query Status message.

Missed Messages

Number

Shows the number messages missed according to the last standard LonWorks network Query Status message.

Neuron Model

One state from a set

Shows the Neuron model according to the last standard LonWorks network Query Status message.

Node State

One state from a set

Shows the state of the node according to the last standard LonWorks network Query Status message.

Offline

True or False

Displays the offline or online status of connected hardware. The LonWorks network server updates this attribute value.

Permanent Status Item Count

Number

Displays the number of items polled as a result of COV signups.

Point Scan Time

Number

Displays the calculated number of seconds the server takes to read all defined points.

Priority 1 Poll Item

Number

Displays the number of items in the Priority 1 list.

Priority 2 Poll Item

Number

Displays the number of items in the Priority 2 list.

Priority 3 Poll Item

Number

Displays the number of items in the Priority 3 list.

Priority 1 Poll Time

Number

Indicates how often the items in the Priority 1 list are polled.
Priority 2 Poll Time

Number

Indicates how often the items in the Priority 2 list are polled.

Priority 3 Poll Time

Number

Indicates how often the items in the Priority 3 list are polled.

Receive Transaction Full

Number

Shows the number of times the transaction full message appeared in the last standard LonWorks network Query Status message.

Reset Cause

One cause from a set

Shows the cause of the last reset according to the last standard LonWorks network Query Status message.

Reset Date

Date

Contains the date stamp of the last local Neuron statistics reset command.

Reset Time

Time

Contains the time stamp of the last local Neuron statistics reset command.

Status Cache Hits

Number

Displays the number of READATTRIBUTE calls that occurred while the object was already being polled.

Status Cache Misses

Number

Displays the number of READATTRIBUTE calls that occurred while the object was not being polled.

Temporary Status Item Count

Number

Displays the number of items polled as a result of READATTRIBUTE calls.

Transaction Timeouts

Number

Shows the timeouts that appeared in the last standard LonWorks network Query Status message.

Transmit Errors

Number

Shows the number of transmit errors that appeared in the last standard LonWorks network Query Status message.

Transmits Per Minute

Number

Displays the calculated number of transmissions per minute.

Version Number

Number

Shows the version number according to the last standard LonWorks network Query Status message.

XIF Present

True or False

Indicates whether the XIF is present. The XIF is a resource file required for the NAE to understand a particular device type. This attribute is not used in the SCT.