External Data Connector integration object - Metasys - LIT-12011964 - Software Application - System Configuration Tool - 16.0

SCT: System Configuration Tool Help

Brand
Metasys
Product name
System Configuration Tool
Document type
User Guide
Document number
LIT-12011964
Version
16.0
Revision date
2023-10-02
Language
English

The External Data Connector object represents a custom client connection such as a MQTT Client connection with the SNx device and the Metasys environment. The object stores the information required to load and establish a functional connection with a compatible custom application.

For further information on how to integrate the MQTT Client External Data Connector object with SCT, refer to MQTT Client External Data Connector Network Engine Commissioning Guide (LIT-12013976).